LTE TDD

UCI Uplink

For Real-Time capability.

This topic describes the settings of the UCI node.

General

PUCCH Common [TDD CC]

Transmission Configuration

General

Enabled

This parameter sets the enable state of UCI. When this setting is turned off, UCI is not be transmitted even if UCI Tx Enabled is ON.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI[:STATe]?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI ON

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI?

Dependencies

If the total number of antennas is 4 antennas, the value is off with read only.

State Saved

Yes

Preset

OFF

Initial S/W Revision

A.14.00

Power

Sets a power level in dB for the selected channel.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:POWer <rel_ampl>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:POWer?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:POW -20.3

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:POW?

State Saved

Yes

Preset

0 dB

Range

-60 dB to 20 dB

Resolution

0.001 dB

Initial S/W Revision

A.14.00

Scrambling

Sets the state of scrambling for the physical channel on or off.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:SCRamble[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:SCRamble[:STATe]?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:SCR ON

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:SCR?

State Saved

Yes

Preset

ON

Initial S/W Revision

A.14.00

RNTI

Sets the Radio Network Temporary Identifier (RNTI) for the corresponding channel transmission.

See 3GPP TS 36.211 and 36.321, for more information.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:RNTI <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:RNTI?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:RNTI 100

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:RNTI?

State Saved

Yes

Preset

1

Min

0

Max

65535

Notes

Range: 0 (0x0000) to 65535 (0xFFFF)

Initial S/W Revision

A.14.00

PUCCH Common [TDD CC]

N_RB(2)

Sets N_RB(2).

This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS 36.211).

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCh:NRB:TWO <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCh:NRB:TWO?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NRB:TWO 2

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NRB:TWO?

State Saved

Yes

Preset

0

Min

0

Max

99 to Maximum resource blocks - 1

Max (LP)

Range: 0 to Maximum resource blocks – 1

0 to 5 (for System Bandwidth 1.4 MHz)

0 to 14 (for System Bandwidth 3 MHz)

0 to 24 (for System Bandwidth 5 MHz)

0 to 49 (for System Bandwidth 10 MHz)

0 to 74 (for System Bandwidth 15 MHz)

0 to 99 (for System Bandwidth 20 MHz)

Initial S/W Revision

A.14.00

N_CS(1)

Sets N_CS(1).

This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS 36.211).

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCh:NCS:ONE <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCh:NCS:ONE?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NCS:ONE 3

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NCS:ONE?

State Saved

Yes

Preset

0

Min

0

Max

7

Initial S/W Revision

A.14.00

nPUCCH(2,0)

Sets the PUCCH format 2/2a/2b resource index nPUCCH(2,0) for antenna port index 0.

Calculated value is nPUCCH(2) < N_RB(2) * N_RB_sc + Ceiling(N_CS(1)/8) * (N_RBsc - N_CS(1) - 2).

See 3GPP TS 36.211, 36.213 and 36.331, for more information.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCH:NPUCch:TWO:ZERO <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCH:NPUCch:TWO:ZERO?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NPUC:TWO:ZERO 1

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NPUC:TWO:ZERO?

State Saved

Yes

Preset

 

Range

0 to Calculated Value (depends on related PUCCH settings)

Initial S/W Revision

A.14.00

nPUCCH(2,1)

Sets the PUCCH format 2/2a/2b resource index nPUCCH(2,1) for antenna port index 1, when the Number of Antennas is 2 Antennas.

Otherwise, it is read only.

Calculated value is nPUCCH(2) < N_RB(2) * N_RB_sc + Ceiling(N_CS(1)/8) * (N_RBsc - N_CS(1) - 2).

See 3GPP TS 36.211, 36.213 and 36.331, for more information.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCH:NPUCch:TWO:ONE <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCH:NPUCch:TWO:ONE?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NPUC:TWO:ONE 1

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:NPUC:TWO:ONE?

State Saved

Yes

Preset

0

Range

0 to Calculated Value (depends on related PUCCH settings)

Initial S/W Revision

A.14.00

Delta Shift PUCCH

Sets Delta Shift PUCCH.

This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS 36.211).

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCH:DSHift <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCH:DSHift?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:DSH 1

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:DSH?

State Saved

Yes

Preset

1

Range

1 to 3

Initial S/W Revision

A.14.00

Group/Sequence Hopping

Sets the hopping type. (Refer to 3GPP TS 36.211)

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCh:HOPPing OFF|GROup|SEQuence

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:PUCCh:HOPPing

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:HOPP GRO

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:PUCC:HOPP?

State Saved

Yes

Preset

OFF

Range

Off | Group Hopping | Sequence Hopping

Initial S/W Revision

A.14.00

Transmission Configuration

This section describes the settings of Transmission Configuration Sequences.

Setting groups of Transmission Config:

Seq 1

Seq 2

…

Seq N

Sequence x

The following settings of the transmission configuration should be set to each subframe configured from the frame length.

The setting dialog of transmission configuration is popped up.

The settings of transmission configuration are shown when the subframe allocation type is Uplink.

Describes the settings of Sequence x, denoting x with the sequence number started from 1.

Notes for SCPI:

SCPI mnemonic TX<n> denotes TX[1]|2|…|<n> where <n> is the configured sequence length.

Frame/Subframe (Type)

Indicates Frame index, Subframe index and Subframe allocation type.

SCPI Command

N/A

Notes

GUI only, Read only

State Saved

No

Preset

"0/0 (Downlink)"

Initial S/W Revision

A.14.00

Frame Index

This number is used to select the target frame number to display setting values.

SCPI Command

N/A

Notes

Query only

This value is indicated in Frame/Subframe (Type) field in GUI

State Saved

No

Preset

0

Min

0

Max (LP)

Depends on Waveform Generation Length

Initial S/W Revision

A.14.00

Subframe Index

This number is used to select the target subframe number to display setting values.

SCPI Command

N/A

Notes

Query only

This value is indicated at Frame/Subframe (Type) field in GUI

State Saved

No

Preset

0

Min

0

Max (LP)

Depends on Waveform Generation Length

Initial S/W Revision

A.14.00

Subframe Allocation Type [TDD CC only]

Indicates the subframe allocation type.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:SFRame:ATYPe?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX3:SFR:ATYP?

Notes

Query only

This value is indicated in Frame/Subframe (Type) of GUI

State Saved

No

Preset

DLINk

Range

Uplink | Downlink | Special

SCPI: ULINk|DLINk|SPECial

Initial S/W Revision

A.14.00

Enabled

Sets the state of the UCI Tx sequence on or off.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>[:STATe] OFF|ON|0|1

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>[:STATe]?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX3 OFF

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX3?

State Saved

Yes

Preset

ON

Initial S/W Revision

A.14.00

Format

Set the UCI format.

Enter a format number for the Tx sequence.

Format 2/2a is not allowed to set in the case Extended CP.

The Modulation type is set by the software based on the selected Format. See Modulation.

The choices available for the HARQ-ACK parameter are based on the selected Format. See HARQ-ACK.

See 3GPP TS 36.211, 36.212 and 36.213.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:FORMat F1|F1A|F1B|F2|F2A|F2B|F3

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:FORMat?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:FORM F1A

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:FORM?

State Saved

Yes

Preset

F1

Range

1 | 1a | 1b | 2 | 2a | 2b | 3

Initial S/W Revision

A.14.00

Modulation

Displays the modulation.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:MODulation?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:MOD?

Notes

Query only

Returns BPSK|QPSK|BQPSk|QQPSk|NA

State Saved

Yes

Preset

 

Range

BPSK | QPSK | BPSK+QPSK | QPSK+QPSK | N/A

BPSK (for Format 1a/1b)

QPSK (for Format 1b/2/3)

BPSK+QPSK (for Format 2a)

QPSK+QPSK (for Format 2b)

N/A (for Format 1)

Initial S/W Revision

A.14.00

Data/Control Type

Sets Data/Control Type.

See 3GPP TS 36.211, 36.212 and 36.213 for more information.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DCONtrol:TYPE?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX DCON:TYPE?

Notes

Query only

Returns HARQ|CQI|SR|CHARq1|CHARq2|CHSR.

State Saved

Yes

Preset

 

Range

HARQ-ACK (for Format 1a),

HARQ-ACK (2bits) (for Format 1b) - the UCI format is set to Format 1b and the UE is configured with a single serving cell, up to a HARQ-ACK (4-bit) channel selection can be set.

CQI (for Format 2),

SR (for Format 1),

CQI+HARQ-ACK (1bit) (for Format 2a),

CQI+HARQ-ACK (2bits) (for Format 2b),

CQI+HARQ-ACK+SR (for Format 3)

Initial S/W Revision

A.14.00

Data

Specifies the data for PUCCH Format 2, 2a, 2b. This setting is readonly for other PUCCH Format settings.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DATA PN9|PN15|USER

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DATA?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:DATA PN15

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:DATA?

State Saved

Yes

Preset

PN9

Range

PN9, PN15, User Defined Bits

Initial S/W Revision

A.14.00

Data User Defined Bits

This setting is used when the data is User Defined Bits.

This setting is shown with the combined entry with Data.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DATA:USER <string>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DATA:USER?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:DATA:USER "00001111"

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:DATA:USER?

State Saved

Yes

Preset

"00000000"

Range

 

Initial S/W Revision

A.14.00

Data Size

Enter a value for Data Size for Formats 2, 2a,or 2b.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DATA:SIZE <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DATA:SIZE?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:DATA:SIZE 10

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:DATA:SIZE?

State Saved

Yes

Preset

 

Range

1 to 13-bits (Formats 2, 2a, 2b with Normal Cyclic Prefix or Format 2 with Extended Cyclic Prefix and CQI Data Type)

1 to 12-bits (Format 2 with Extended Cyclic Prefix and CQI + HARQ-ACK (1-bit) Data Type)

1 to 11-bits (Format 2 with Extended Cyclic Prefix and CQI + HARQ-ACK (2-bits) Data Type)

Initial S/W Revision

A.14.00

HARQ-ACK

Specifies the HARQ-ACK information corresponding to PUCCH Format 1a, 1b, 2a, 2b and 3. This setting is readonly for other PUCCH Format settings.

The choices available for HARQ-ACK are determined by the active Format.

Refer to 3GPP TS 36.211, 36.212 and 36.213.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:HARQ ACK|NACK|ACKACK|ACKNACK|NACKACK|NACKNACK|ALLACK|ALLNACK|USER

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:HARQ?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:HARQ NACK

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:HARQ?

State Saved

Yes

Preset (LP)

ACK (Format 1a/2a)

ACK-ACK (Format 1b/2b)

ALL ACK (Format 3)

Range

ACK | NACK | ACK-ACK | ACK-NACK | NACK-ACK | NACK-NACK | ALL ACK | ALL NACK | User Defined Bits

ACK | NACK | ACK-ACK | ACK-NACK | NACK-ACK | NACK-NACK | ALL ACK | ALL NACK | User Defined Bits

ACK | NACK (Format 1a/2a)

ACK-ACK | ACK-NACK | NACK-ACK | NACK-NACK (Format 1b/2b)

ALL ACK | ALL NACK | User Defined Bits (Format 3)

Initial S/W Revision

A.14.00

HARQ-ACK User Defined Bits

This setting is used when HARQ-ACK is User Defined Bits.

This setting is shown with the combined entry with HARQ-ACK.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:HARQ:USER <string>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:HARQ:USER?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:HARQ:USER "00001111"

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:HARQ:USER?

State Saved

Yes

Preset

"00000000"

Range

String consisting of 0 and 1

Initial S/W Revision

A.14.00

nPUCCH(1,0)

Sets a value for the PUCCH n(1) number.

Specifies the resource index for PUCCH formats 1/1a/1b.

Calculated maximum value means the resource is at the center of the system bandwidth.

Refer to 3GPP TS 36.211, 36.212 and 36.213.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:ONE:ZERO <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:ONE:ZERO?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:ONE:ZERO 10

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:ONE:ZERO?

State Saved

Yes

Preset

0

Min

0

Max (LP)

minimum (2047 or Calculated Maximum Value) <- Ayumi ? Smaller of 2047 or Calculated Maximum Valueの意味でしょうか?(depends on the related PUCCH values)

Initial S/W Revision

A.14.00

nPUCCH(1,1)

Sets nPUCCH(1,1).

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:ONE:ONE <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:ONE:ONE?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:ONE 1

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:ONE?

State Saved

Yes

Preset

 

Range

 

Initial S/W Revision

A.14.00

nPUCCH(3,0)

Sets a value for the nPUCCH(3) number.

Specifies the resource index for PUCCH format 3.

Refer to 3GPP TS 36.211, 36.212 and 36.213.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:THRee:ZERO <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:THRee:ZERO?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:THR:ZERO 1

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:THR:ZERO?

State Saved

Yes

Preset

0

Range

0 to (Number of resource blocks in the system bandwidth) * 5 – 1

Initial S/W Revision

A.14.00

nPUCCH(3,1)

Sets nPUCCH(3,1).

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:THRee:ONE <integer>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:NPUCch:THRee:ONE?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:THR:ONE 1

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:NPUC:THR:ONE?

State Saved

Yes

Preset

 

Min

 

Max

 

Initial S/W Revision

A.14.00

RB Location (TDD CC only)

Displays the numbers of the resource blocks occupied by the PUCCH, separated by a comma. If any of the following are changed: PUCCH Format, N_RB(2), N_CS(1), n(1), n(2), Delta Shift or Delta Offset, the resource block numbers are updated accordingly.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:RB:LOCation?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX:RB:LOC?

Notes

Query only

State Saved

No

Preset

 

Range

 

Initial S/W Revision

A.14.00

DMRS Power

Sets a power level in dB for the demodulation reference signal for the UCI Tx sequence.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DMRS:POWer <rel_ampl>

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:TX<n>:DMRS:POWer?

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX3:DMRS:POW -10dB

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:TX3:DMRS:POW?

Notes

Unit in GUI: dB

State Saved

Yes

Preset

0 dB

Min

-60 dB

Max

20 dB

Resolution

0.001 dB

Initial S/W Revision

A.14.00

Tx Configuration Tools

Import Tx Config

Command Type

Immediate Action

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:IMPort <string>

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:IMP "UCITX.txt"

Notes

Set only (Immediate Action)

State Saved

No

Preset

 

Range

 

Initial S/W Revision

A.14.00

Export Tx Config

Command Type

Immediate Action

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform:RTIMe:CCARrier<carrier>:ULINk:UCI:EXPort <string>

SCPI Example

:RAD:LTET:WAV:RTIM:CCAR:ULIN:UCI:EXP "UCITX.txt"

Notes

Set only (Immediate Action)

State Saved

No

Preset

 

Range

 

Initial S/W Revision

A.14.00

Column Preset

Set one value to a target parameter of all subframes, like Set all “State” to On, or Set all “Format” to 1b.

Command Type

Immediate Action

SCPI Command

N/A

Notes

Set only (Immediate Action)

State Saved

 

Preset

Refer to the element definition of the data part below.

Range

Refer to the element definition of the data part below.

Initial S/W Revision

A.14.00

Preset Setting Name

Selects a setting name to preset.

SCPI Command

–

SCPI Example

 

Notes

Set and Query

GUI label: Column

Value Selection: Pulldown menu

State Saved

No

Preset

Enabled

Range

Refer to the element definition table in Column Preset section.

Initial S/W Revision

A.14.00

Preset Setting Value

Selects a value to preset for the selected setting.

SCPI Command

–

SCPI Example

–

Notes

Set and Query

GUI label: The name of selected setting in Column

Value selection: Depends on the selected setting. Refer to the section of the selected setting

State Saved

No

Preset

Depends on the selected setting. Refer to the section of the selected setting

Range

Refer to the element definition table in Column Preset section.

Initial S/W Revision

A.14.00

Carrier Uplink ARB

Carrier Uplink Real-Time

Welcome to LTE TDD